AXIS#.MOTOR.RTYPE
Description
This parameter defines the type of thermal resistor used inside of the motor to measures motor temperature. See Motor Temperature for the supported thermal resistor types.
-
-
This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET=1 and motor memory version is 0.3 or greater.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 8, 127, 255 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.MOTOR.RTYPE | 0x500B | 0x19 | USINT | - | - | RW | False |
| AXIS2.MOTOR.RTYPE | 0x510B | 0x19 | USINT | - | - | RW | False |